Tool/software:
I know this isn't Tina-TI, but still, TI should know about it. I just paid $197 for Tina14, with an online download from designsoftware.com, and installed it on a 2023 M2 Mac mini running Sonoma 14.5. It won't install fully using the Wineskin software that came with it, but will install under Crossover.
Just for the halibut, I modified an old, old "Absolute Value" circuit, from page 69 of the 1963 Burr Brown "Handbook of Operational Amplifier Applications", with two diode and RC low-pass filters for attack and recovery on a single capacitor. Pretty simple stuff. I'm looking at several different designs, this being not the best.
The Tina14 "Oscilloscope" tool seems to work OK, but the "Multimeter" doesn't. I'm varying the 50 Hz source voltage from 1 Vpp down to about 20 mV pp. In one instance, the multimeter measured a node of 38.8 V AC. Besides that, the multimeter measures the DC voltage on the capacitor as being on the order of E-17 volt. These are non-physical results. When I brought this to the attention of Design Software, the online tech told me that because the multimeter is a linear device and the diode circuit is nonlinear, it won't work.
Silly me. In my reply, I pointed out that a sine curve is nonlinear, but undergrads still learn how to calculate RMS voltage.
Can Texas Instruments recommend a more reliable simulation package? One that works on MacOS?