Part Number: PMP41062
Other Parts Discussed in Thread: BQ25756, TPS25751
Tool/software:
Hi team,
I have two questions as below. Look forward to get your insight on these.
1.
There is two power supply for PD (3.3V/5V) from the reference schematic. Battery > 5V Buck converter > LDO 3.3Vout
What is the purpose of the 5V Power supply? Is it required for 3A Load switch operation? If I don't use the load switch, can I remove it?
I am wonder if CC power also requires this 5V pull up power.
2.
Is TPS25751+BQ25756 can support charging + discharging with one path? It seems charger supports the bi-directional but I am not sure if this ref. board support one path charge/discharge as well.
3.
I am doing project (power bank) which should support battery power (12~18V), USB output power (5/9/12/20V) as below table.
Should I add load switch for this application? or just connect two port to VBUS?
|
Voltage |
Port1 (USB-C) |
IN: 5V/3A, 9V/3A, 12V/3A, 15/3A, 20V/3A, 20V/5A |
|
Port2 (USB-A) |
OUT : 5V/4.5A, 9V/2A, 12V/1.5A |