Part Number: PMP41042
Other Parts Discussed in Thread: TMS320F280039C, TIDM-02013
Tool/software:
Hello
We are starting with new design BESS. Input voltage 230VAC, output voltage 48V, output power 3KW. PFC topology is single phase CCM Totem pole with switching frequency 70Khz. DC/DC stage topology is CLLLC with configuration Full bridge on primary and secondary side. Resonant switching frequency of DC/DC stage is 130Khz. We want to controll both stages with only one single controller TMS320F280039C. Do you think it is good idea or you recommend controller with higher class?
Thank you