This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010210: 11KW OBC Charger

Part Number: TIDA-010210

Tool/software:

Hi TI Team,

Kindly suggest best way to proceed for design of 11KW on board charger

Input is 3 Phase, Output is 240V to 470V DC

can i use analog controller IC for PFC operation,what difference does it make for digital controller

DC-DC, can i use Phase shifted Full Bridge(PSFB) for DC-DC stage

Thank you

venkatesh  B