Part Number: PMP23333
Other Parts Discussed in Thread: LM61495, TPSM63610
Tool/software:
Hi support team,
I am looking for a device that can be used with the following plan.
Plan-1
Vin : 6.5V
Vout : -6.5V
Iout : 3.0A
Plan-2
Vin : 5V
Vout : -5V
Iout : 2.6A
Is it possible to achieve this using PMP23333 with LM61495?
Plan-2 is possible with the TPSM63610, but Plan-1 seems difficult.
www.ti.com/.../snvaa71
Regards,
Dice-K