Part Number: TIDA-010050
Tool/software:
We are using TIDA-010050 to create a water meter monitoring device. We incorporated TIDA-010050 design into our own design, and created a monitoring device. We are testing the TIDA part now.
Test setup:
Texas chip from the reference design TIDA-010050 with Sensor Controller Studio software. Water meter is equipped with custom enclosure to hold our device on the flag.
My questions are the following:
- How can we fine tune the system for our needs? Is REFDAC_OFFSET what we need to increase or decrease to find the optimal point for the detection?
- Does time affect the detection? It seems, that if we start the water meter before starting the software, it is fine, but if the software runs for 20-30sec, the calibration is different, and so are the measured values and the sensitivity.
- How can we add a third coil to the system? We designed our panel with three coils, but we want to include the third one. Can we do it by changing a #define or should we rewrite the code?