Part Number: TIDA-010049
Tool/software:
Hi Ti expert,
TIDUEN7 Figure 5 lists 6 types of fault which TIDA-010049 can detect.
My questions is:
If the digital inputs of one product needs to meet IEC61508-2:2010(SIL2) and EN13849-1:2015 (Cat2 PLd) , does the product must be able to detect the 6 types of digital input wiring faults? Is this required in IEC61508-2:2010(SIL2) or EN13849-1:2015 (Cat2 PLd)?
Thank you in advance.