Other Parts Discussed in Thread: TPS54560, TPS54560B,
Tool/software:
Hii TI Team,
I was using similar schematic for my design to convert 5- +/- 40 V conversion.
Initially, i have used DC supply of 0-32 V , 2 A and tried to provide input of 5 V to get +/-40 V at the ouput. Once reaching 4.3 V supply is going to CC mode.
Further as the current limit for the regulated DC supply was 2 A only but the test results provided by TI shows that at input of 4.847 V has input current up to 2.585 A and efficiency being 80.7% hence replaced DC supply with other supply with 3A rating ...other channel with max 5A rating .. what i can see is current limit should be high when input is slowl increased from 0-5 V untill we reach this 5 V , the supply is going to CC
Even tried 5 V, 5 A channel to provide input but i can see IC TPS54560 heating faster and i have shutted down.
Each resistor, capacitor are fine as per mentioned values, ICs are also fine still not able to obtain +/-40 V at the output.
Also using DPO probed the input values, i can see only input voltage appearing at 2(VIN) to GND and 3(EN) to GND... no voltage at any of other terminals .
Kindly help... I hope i have elaborately told the issue


boot and SW pins shows some switching noise type waveform with peak-peak 2 V like that ... the shape shown above