Other Parts Discussed in Thread: UCC28950, UCC27714, UCC28070, UCC28180
Tool/software:
Hi TI Experts,
Please suggest a DC-DC topology for a 1.2kW power supply that intakes a PFC output of 400V.
There are a few requirements for the design as listed below:
1. Maximum current 15A.
2. Voltage between 30V to 80V, which can be programmed by MCU.
3. Is there any preferred PFC topology for the above mentioned requirements.
Would like your valuable insights on the same.
Thanks & Regards
Mohammed Ibrahim