Part Number: UCC3895
Tool/software:
Hello Mike O',
First, many thanks for your reply.
About the control mode, I think that with my application I would use voltage mode control. It's a high ratio converter (x30) and for the closed loop regulation, the voltage reference is the input voltage.
The variation range of the input voltage is between 10 and 80V. Do you think that the voltage mode regulation is suitable?
When you talk about the transformer, do you mean the current transformer ? Do you have an idea about DC blocking capacitor value in series with the transformer to prevent transformer saturation ?