Part Number: TIDA-01600
Other Parts Discussed in Thread: DRV8329, ULN2003A, TPS27S100
Tool/software:
Hi Team,
I have a quick question about the use of J5 in TIDA-01600.
1. J5 is used for break coil connection. However, there were no MOSFET. How to connect directly to one of the brake wires? And if a wire is connected to J5, where should the other brake wire go?

2. I couldn't find the necessary parameters to switch the high-side and low-side MOSFETs at my desired frequency, particularly for the TPS27100APWR. Can I determine the output frequency based on the frequency I provide to the high and low inputs, similar to how I do with the DRV8329?
Thank you and Regards,
Marvin Arcangel