Part Number: PMP41042
Tool/software:
Hi team,
Regarding to PMP41042, is it possible to control three to four parallel systems when dealing with higher power?
Specifically, the following configurations are considered.
Input: 50VDC, 180A
Output: 320VDC, 28A
Best regards,
Goto