This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61378-Q1: TPS61378-Q1

Part Number: TPS61378-Q1
Other Parts Discussed in Thread: TINA-TI

Tool/software:

Hi, please help me with this

I want to import the TPS61378-Q1 to TINA-TI , PSpice Downloadable file is present on website of TPS61378-Q1

Please share the steps or the TINA-TI file for TPS61378-Q1

  • Hi, there is an updation on the above question.

    I am able to import the PSPICE model to TINA - TI, 

    TPS61378-Q1, in the downloadable files, encrypted version is available. PLEASE KINDLY SHARE THE UNENCRYPTED VERSION PSPICE FILE of TPS61378-Q1, i am getting error $CDNENCSTART_ADV2.cLine: #31. Also .tld file is not available, .lib is there, the TINA-TI is warning, equal number of .tld and .lib file should be there. Kindly share the unencrypted .lib file which says TPS61378Trans_Encrypted.lib.

  • Hi Himagowri,

    Sorry for TPS61378-Q1, only the encrypted PSpice model is available and provided.

    We suggest that you may use the PSpice for TI for your simulation.

    PSpice for TI can be downloaded from TI official website and it's free.

    Regards

    Lei

  • Hi Lei Zhong,

    " PSpice for TI " is the one which has encrypted files 

    I am trying to import the PSpice mode to Tina-TI, due to encryption of the file, i am not able to.

    Is there any way you can help me get the unecrypted .lib file of TPS61378-Q1 please ?

    I followed these steps in TINA-TI to import the macro TPS61378-Q1

    i) new macro wizard, and then paste the .lib encrypted file and name the macro

    ii) click on next , and load the shape from library

    ii) Connect the pins to the design 

    iv) NOW here when i click next, i get $CDNENCSTART_ADV2.cLine: #31 and i am not able to proceed

    All this i did using PSpice for TI file which i downloaded from website

    Kindly help me with this

    Thanks and regards

    Himagowri V

  • Hi Himagowri,

    For TPS61378-Q1 there is no unencrypted PSpice model.

    I suggest that you can use the PSpice for TI to run the simulation on the encrypted PSpice model.

    Regards

    Lei

  • Thank you Lei Zhong , i will use the PSpice tool

    Regards

    Himagowri V