This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010254: the power consumption consideration for the battery system

Part Number: TIDA-010254

Tool/software:

Dear team,

our customer want to follow the TIDA-010254 to design their Lidar sensing product.

however we are curious about the how the system help with power saving. in the following table in the design guide:

how we get the system power consumption 180mW parameter here, is it based on the calculation or measurement?

if this is based on the calculation, may I know how we estimate the power consumption caused by the TI components.

we have a wanted using scenario, which is the sensing procedure awake 10 time per day, each time will last 1 minute .

the system is powered by 18650  single battery cell. how we can apply the power consumption 180W into this scenario's battery life estimation? will the inrush current of system wake-up need to be considered?

Best regards,

Hank Lin