This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM843320: TPSM843320 webench simulation model for load transient

Part Number: TPSM843320

Tool/software:

Hi Team,

I am using the TPSM84362 part in my design with the following configuration:

Input voltage: 12V

output voltage: 1.8V

load current: 2A. and 0.03A

Since Webench simulation is not available for this configuration, could you please assist me with the simulation model?

Thank you!