Tool/software:
I'd like to check compliance against the MIL-STD 1275F. In this release of MIL STD, Injected voltage surge event#2 was added, with a load dump pulse of 100V and 500ms duration.
The new load-dump pulse specifies 5 × 500-ms pulses over 25 seconds that is more severe than the 50-ms load-dump specification in the previous standard.
Is TIDA-010242 qualified also for Injected voltage surge accordingly. The reference design states compliance with the MI-STD1275E.
If not, do you intend to upgrade the product ? If you have some information for me, would be very helpfull to pursue a product development.
Regards.
Nada