Part Number: PMP23338
Other Parts Discussed in Thread: PMP23069
Tool/software:
Hello,
I am trying to bring up the PMP23338(using Hall sensor) from light load with the High Flux C058894A2HT19 core(46Turns of AWG18) for the Boost Inductor (as mentioned in the Test Report of PMP23338 )
However while load testing at high line(230Vac) as we reach higher loads where the output current reaches 7.75Amps(Po = 2.95kW), the inductor current waveforms start getting distorted at the peaks and the inductor starts making noise:

(Inductor Current IL at 230V Highline Input, 7.75Amps)
Further, I wounded 60 turns and then got these similar behavior at 8.7Amps output current(Po = 3.3kW)

(Input Current Iin_rms at 230V Highline Input, 7.75Amps)
How many turns on C058894A2HT19 have been wounded to reach 3.6kW(9.4Amps without inductor current waveforms getting distorted)
Currently, the EMI section of the board is shorted(non populated) could it be affecting these current waveform/behavior/ of the PFC Inductor?
Regards,