Part Number: TIDA-01605
Tool/software:
Hi,
What would be the maximum gate driver output current for the TIDA-01605? I am asking because, the transformer T1 power is 1 W, and the secondary current is 50 mA. The gate driver U6 peak output current is 6 A, but the input current (net: +15Va) is only 50 mA. The back of the envelope calculations for the MOSFET I am planning to use give a turn-off current of 1.68 A, so 6 A should be more than sufficient. However, based on the components on the board, I am not sure even 1.68 A is achievable. Can you please confirm if this is correct or I missed something?
Thanks, MB