This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP8877: Power solution recommendation

Guru 12825 points

Part Number: PMP8877

Tool/software:

Hello,

My customer is looking for a power design solution that can meet the requirements below:

  • Input voltage: 57V
  • Output voltage: 12V
  • Current: min 15A
  • Efficiency: min 94%@8A, room temperature
  • Isolated type, Within 1/16 brick

If there are any solutions or reference designs among TI products that meet customer requirements, please recommend it.

Thank you.

JH