Part Number: TIDA-01081
Other Parts Discussed in Thread: TPS92515HV
Tool/software:
I am very interested in driving this reference design LED string voltage at 42V. Is this possible?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-01081
Other Parts Discussed in Thread: TPS92515HV
Tool/software:
I am very interested in driving this reference design LED string voltage at 42V. Is this possible?
Hello. The TIDA-01081 rating = 24V, 2.4A.
Ideally, I wish to use one TIDA-01081 board to drive two 42V, 1.2A LED panels. I think this is = 42V at 2.4A?
Alternately, I could use just one 42V, 1.2A LED panel.
But, the LED driver (TPS92515HV ) is rated up to 65V, and two LED panels would be fantastic!
So, is it possible to change or add components and keep the circuit largely unchanged?
Much appreciate any insight!
Hi Fran,
The major component for controlling the LED current value is the TPS92515HV which is rated for a max recommended and absolute max VIN of 65V . I would preferer to stay slightly below this max value ...
The TIDA-01081 uses for the TPS92515HV a max VIN of 49V for electrical safety purposes (during testing in the lab) - can therefore be increased in a real customer application with a customized design. The LED string voltage can also be increased to 48V, provided that the VIN of the TPS92515HV is larger than the string voltage and that the design is customized to it. It is basically the difference between this VIN and the LED string voltage which drives how fast the inductor (L1) current can rise - please see fig 27 and table 8 in the user guide . However: all such changes will have consequences on a lot of different circuit blocks and subfunctions in the circuit. All the circuit blocks needs to be carefully checked and if needed customized for the higher voltage levels. There are overvoltage protections implemented in many of the circuit blocks, which would otherwise be triggered - in hardware, but also in the software of the MCU. Not to forget: Beside the voltage limitations there are also power limitations (voltage depended current limits) in hardware and software implemented (examples for that are Common Power and the Pre-Boost circuit blocks).
Excellent reply, thank you for the very helpful insight.
Knowing that the TPS92515HV and the LED string voltage handle up to 48V is a big help. And great suggestions of other areas to adjust. To start testing, I'll likely short half my LED board and alter it to 21V 2.4A. Then start customizing!