Tool/software:
Hello, thank you. The TIDA-01081 board is rated = 24V, 2.4A.
But, ideally, I want to almost double the voltage = 42V, 2.4A.
Alternately, I could use 42V, 1.2A.
Our beefy "HV" LED driver (TPS92515HV ) is rated up to 65V.
What do you think? 42V, 2.4A drives two LED panels and would be fantastic!
So, is it possible to change or add components and keep the circuit largely unchanged?
Much appreciate any insight!