Part Number: TIDA-020033
Other Parts Discussed in Thread: TAS6584-Q1, LM5143
Tool/software:
Hi team,
I want to know if it is possible to use a buck controller(e.g. LM5143) to make a Class-H tracking power supply for TAS6584-Q1? It seems we only have reference design with boost controller, but I guess buck controller may have a similar design to support Class-H function. Is there any concern to use buck controller for Class-H?
Our customer has both 48V and 12V power supply on their board, so they can use buck controller to get a 20V PVDD from 48V input for TAS6584-Q1, which seems to have better efficiency than boost topology.
Customer requirement:
- Input: 48V or 12V
- Output: 45W x4 speakers
Thanks,
Muwei Zheng