This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP22504: シミュレーション、ハードウェア、システム設計ツールフォーラム

Part Number: PMP22504

Tool/software:

As for the specific application, I am planning to set the torque and rotational direction of the torque motor (2TK3A-AW2J) through the power controller (TMP-1).

  1. Separate the existing AC vibration data D(t) into two types of signals: the absolute value of the amplitude A(t) and the signal that distinguishes between positive and negative amplitudes B(t).

  2. Use an operational amplifier to amplify the voltage of B(t) to 24V to match the specifications of the power controller.

  3. For the amplified B(t), I need a product or IC that can output the signal from one terminal when the signal is positive and from another terminal when the signal is negative.

  4. Connect the positive signal to the CW (clockwise) terminal of the power controller and the negative signal to the CCW (counterclockwise) terminal, ensuring that the signal flows accordingly.

  5. Simultaneously pass A(t) to set the torque and rotational direction, and output the vibration of D(t) via the motor.

Currently, I am searching for a product or IC that can accomplish step 3.

I have attached the relevant pages from the torque motor's power controller manual and a diagram of the process outlined above.