Part Number: LMR16006
Tool/software:
Hello TI Team,
We are designing the following power supply circuit using IC: LMR16006YDDCR, however we found a discrepancy between the specs in the datasheet and the TI Webench simulation.
1. Design requirements:
+ Input: 18 – 45Vdc
+ Output: 5Vdc / 0.6A
2. If based on the datasheet, this design is feasible, shown in Figure 7: Line Regulation on page 7 of the datasheet (Figure below):

3. However, when I run the simulation on TI Webench and fill in the parameters of item 1, TI Webench reports an error as shown below

Final question: Can we use IC: LMR16006YDDCR for DC-DC power design with input 18 - 45Vdc and output 5Vdc/0.6A?