This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28600: UCC28600: Simetrix simulation failed with the imported SPICE model

Part Number: UCC28600

Tool/software:

Hi,
For one of our application we are using UCC28600. As a part of design activity we tried to simulate the design using Simetrix tool but we are getting the error like  "
Unknown model type 'UGATE'", "Cannot find definition for model 'IO_4000A', (line ref ucc28600.lib,32)". Need support to resolve the issue.

Note : I have used the Un encrypted library model for the simulation.