This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA on Windows 7 Enterprise version

Should TINA run on Windows 7 Enterprise version?  After a lengthy simulation (30+ minutes -- sometimes earlier or later), TINA goes "non responsive" and I get an ApplicationHangError.

  • This is what ERROR detail looks like:

     

    Problem Event Name: AppHangB1

    Application Name: TINA.EXE

    Application Version: 9.3.30.248

    Application Timestamp: 2a425e19

    Hang Signature: 482c

    Hang Type: 0

    OS Version: 6.1.7601.2.1.0.256.4

    Locale ID: 1033

    Additional Hang Signature 1: 482cb1d780ef9440e4a611f2a79f5287

    Additional Hang Signature 2: 776b

    Additional Hang Signature 3: 776bc08415675b44eb19db27655b31d1

    Additional Hang Signature 4: 482c

    Additional Hang Signature 5: 482cb1d780ef9440e4a611f2a79f5287

    Additional Hang Signature 6: 776b

    Additional Hang Signature 7: 776bc08415675b44eb19db27655b31d1

  • Thanks for the report. I've sent it off to the developers to see what they have to say.

  • TINA works fine with all versions of Windows 7 including the Enterprise version; the developers report  they regularly use the Enterprise version, along with testing on most other Windows platforms. 
    Can you share your circuit with us? (Post a zipped version of your .tsc file) The developers suspect this may be a problem in the circuit file or with a particular model.

  • Yeah, it is most likely a Windows 7 Enterprise problem as the same model works on four XP computers.  If I set TINA in "compatibility mode" on the Windows 7 Enterprise machine, it is more reliable, but rather than becoming non-responsive as posted before (with the Windows error details), it may lock up silently.  The problem is with very long transient simulation and doesn't occur for 40 or so minutes of execution time (on an i7 box).

  • As further update of compatibility issues between TINA SPICE and Windows 7 (in compatibility mode), I have recently been battling cases where my transient simulation runs 50% through its 420uS run and causes a "floating point" or "floating point overflow" error.  In the latest failure, the simulation ran for some time (approximately as mentioned before), then I got an error stateing "Exception EAccessViolation in module update.exe at 42E82000.  Access violation at address 42E82000.  Read error at address 42E82000.

    The same model simulates on Windows XP Professional just fine.

    Very frustrationg

  • Sorry to hear that. Again, if you can send us the .tsc file maybe we can help find the issue. Not sure what else to do at this point. If you don't feel comfortable posting the file, send to me via e-mail at downs underscore rick at ti dot com.

  • I will check about the sensitivity to sending the model.

    Still, like I said before, the model runs on four other computers (including multi core computers) all running Windows XP Professional, so it is diffult to understand how this is a model problem.  I did have floating point over flow problems with Tina Pro and it was fixed (revised about a week ago), but that fix didn't happen on TI TINA as its last revision date is early September.