Part Number: TIDA-00366
Tool/software:
Hi,
In TIDA-00366 reference design, the grounding scheme is such that the reference points (U_BOT_REF, V_BOT_REF, and W_BOT_REF) are connected together to VDC- through 0-Ω resistors R133, R139, and R140 respectively. They are also connected with the GND1 (ground for a 16-V gate-drive power supply) through one more 0-Ω resistor R142.
It implies that each of the bottom side Gate driver Gnd is connected to Gate driver Power supply Gnd and to VDC- thorugh the 0ohm shorting links on the PCB.
I have couple of questions on this arrangement
- What is the use of this shorting link? Why not directly connect all the bottom side 3-Ph gate driver section Gnd through some common star point in the layout routing itself?
- Which is a better grounding scheme in case of external Power modules with external AC and DC busbar arrangement
a) Connecting all the bottom side grounds of Gate driver section together through shorting links/layout in PCB
OR
b) Keeping the Gnd Plane of all the bottom side Gnd separate on PCB as they ultimately get connected through the VDC- busbars?
3. In continuation to question 2, what if individual power supplies were given to bottom side gate drivers. Do we need to connect its Gnd together on PCB or tie it at one end on PCB OR should we keep the ground plane of each of the bottom side gate driver phase separate and then it gets connected externally through VDC- busbars?