Part Number: TIDA-080004
Tool/software:
Hi Champs,
Now customer use TIDA-080004, and now they have requirement on cyber security: It is necessary to disable all unnecessary hardware external interfaces (such as JTAG, UART, I/O, USB, etc.) to protect the data in the memory, and ensure that there are no hidden interfaces for illegal access. And need secure boot to avoid attacking the system through external interfaces.
I think F28023 doesn't support this, so how can we meet customer's this requirement?
Thanks!
Julia