This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR51420: Very long simulation time

Part Number: LMR51420

Tool/software:

PSpice simulations are running very slow on the new laptop.

Simulation times for same project:

Old laptop Win11:   Intel XEON W-10885 CPU @ 2.40GHz Simulation time 30 minutes.

New laptop Win11: 13th Gen Intel Core(TM) i9-13950HX    Simulation time 2 hours 45 minutes! Utilization 17%, 2,52GHz

PSpice does not use available cores.

Increasing Options/Threads to 8, 10, 20, 200 has no effect at all.

Why is PSpice using approx. 3 cores of 32 cores?