This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8686SEVM-PDK: Microvolt Signal Reading with ADS8686SEVM-PDK Board

Part Number: ADS8686SEVM-PDK
Other Parts Discussed in Thread: ADS8686S

Tool/software:

Hello,

We are attempting to read microvolt-level signals with the Texas Instruments ADS8686SEVM-PDK development board. I am attaching screenshots of the signal we send from the signal generator as well as the signal we read through the interface, along with an image of our test setup.

The signal we read from the interface appears with a DC offset. Is there a way to adjust the parameters in the GUI to resolve this, or is this issue only solvable through hardware modifications? Additionally, when we log the data, the Excel file shows values rounded to limits like 0, 1, and 2. How can we modify the format of this log file?

Lastly, do you have any source code available that would allow us to use a GUI similar to yours and transfer data from the registers to a PC via UART?

Thank you in advance for your support.

Best regards,

   36dB_deneme_07_11_24_11_03_43.csv