This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP22650: Customer queries regarding best current sensing method

Part Number: PMP22650

Tool/software:

Hello Team,

.1. Can customer use Hall based current sensors to sense the high frequency CLLLC Primary & Secondary current ? If not then suggest any part No. or method.

2. Is the secondary side current (low voltage DC side) being used as a parameter in the Control algorithm of Charger or just primary side high frequency current sensing would be enough for the Charger operation?

Regards,

Jinesh

  • Hi, Jinesh,

    Yes, it may be possible to use a hall sensor for the LLC control. TMCS1133B1QDVGR might work, however, you'd need to consider the bandwidth and if it would be sufficient for the application. 

    Alternatively you could use a current sense transformer. I don't know a part off hand that would fit the application.

    The unit uses the output current for control when operating the power supply as a current source.

    Best regards,

    Brent