Tool/software:
Hi,
I'm trying to follow the TIDA-010272 (TIDUF88 – OCTOBER 2024), specifically the part related to the Insulation Impedance Monitor, under section 2.2.3.
The equations (2) and (3) do not seem correct. I created the circuit as presented in Figure 2-4, and followed the configurations set by the steps 1 to 4 in that section, and the numbers I get do not match the values from the equations. Could someone confirm the steps and the equations in that section are correct?