This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP41062: TPS25751 become a sink when connect to cell phone

Part Number: PMP41062
Other Parts Discussed in Thread: BQ25756, TPS25751,

Tool/software:

We use TPS25751 in battery bank design. We also have a BQ25756 between TPS25751 and battery. We find when we remove the battery and the output connect to cell phone. Then the Bat+(charger output) has 42V voltage. It seems that the cell phone become a source. Even we had test the only 5V type-C adapter without CC analog. It has the same behavior. 

We don't want the cell phone become a source. May I know how to do that? Thanks

Battery voltage: 30V to 40V

Battery open is 42V.

Type-C input: 5V or 9V

BR,

Gary