Part Number: PMP10088
Other Parts Discussed in Thread: TPS54360
Tool/software:
Hi,
Can you verify the following schematic for ±15V supply:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I do not know the maximimum load current and the max neg. current of the the TPS54360 but schematic looks okay so far. I would recommend to place the pole to half of the switching frequency by changing Cpole 120pF. BTW, there is an application report for creating a split rail power supply which could be helpful:
https://www.ti.com/lit/an/slva369a/slva369a.pdf?ts=1733319843774
regards,
Flo