This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00702: AC Current Source

Part Number: TIDA-00702

Tool/software:

Hi,

I am looking for a stand-alone module solution that can generate AC (50-60Hz) current source/sink on the range of about 1mA to 100mA and 1uA to 1000uA (or 100mA to 6A and 5mA to 800mA).

The desired current value being programmable.


My application requires sensing the latter current levels and I need something to test it with.

Something cheaper than programmable AC power supply or AC electronic load and with only small current range (uA, mA).

(Part number above is only to complete the required fields and not necessarily related to this question.)

Thanks