Part Number: TIDA-01606
Other Parts Discussed in Thread: AMC1306M05,
Tool/software:
Hi team,
1.We found that the voltage of TINV_vBus_sensed_Volts was high when using lab2
Is the voltage of the other 3-phase TINV_vGrid_A_sensed_Volts TINV_vGrid_B_sensed_Volts TINV_vGrid_C_sensed_Volts low?
Can this be adjusted?
2. #Define TINV_ADC_PU_SCALE_FACTOR ((float32_t)0.000244140625)
Is this vref at 1.0v? But is the control card not 3.0 v?
When testing lab5, if the input frequency is greater than 65, the voltage current is not measured? Can this be adjusted?
Thank you for your help :D.
Best regards,
Jiahui