This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010054: Reverse operation

Part Number: TIDA-010054

Tool/software:

Hi Team,

Our customer would like to know if he can use the secondary side of TIDA-010054 as primary and its primary side as secondary.

The primary voltage range of TIDA-010054 is 700V–800V DC while the secondary voltage range is 350V – 500V DC (SPS) 250V–500V (EPS). The customer has a voltage source of 350VDC ~ 500VDC and wants the output voltages be 700VDC ~ 800VDC

Regards,

Danilo