This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01606: Part number 3PH Inverter 3kW

Part Number: TIDA-01606


Tool/software:

I'm searching for a module to control a 3-ph Motor acting as Inverter. The power required is 3KW, phase current up tp 20A.

We must start from the 400V 3-ph, apply a first AC/DC conversion to manage the V supply for sensors, MCU and and also a 48V(?) to drive the inverter controlling the Motor.

Is the TIDA-01606 a suitable pn? 

Is there any other pn or referecne design?

Also, the availability of an Evaluation Kit will be useful.

Thank you

Daniele Cavazza