This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010936: Help to check if TIDA-010936 reference design could support PMSM motor

Part Number: TIDA-010936


Tool/software:

Hi Team,

Could you please help to check if TIDA-010936 could support PMSM motor? And if your team could help to use this reference design give a test of customer motor to see the efficiency and thermal? Customer is doing a research platform with 500W output, and the Vbus voltage is 25V. Thanks a lot for your support to check.

Best regards

Jie

  • Hi Jie,

    Thank you for reaching out to us on this case.

    The TIDA-010936 is a power stage reference design and can be used for any 3-phase motor driving including PMSM.

    For a specific customer support case, let's discuss it offline.

    Best regrads,

    Jerome Shan