Part Number: UCC28750
Tool/software:
I am designing a 150W Flyback converter with 85VAC-265VAV input and 24VDC-6A output using IC UCC287502.
When I supply 15V DC voltage to the VDD pin of the IC, the converter works stably, 15V I get from an external voltage source.
When I run the converter with the IC, without 15VDC for VDD, I use the Aux coil for the VDD pin of the IC and start it with a 3MOhm start up resistor. However, when starting up, the output voltage does not reach 24V and the auxiliary winding voltage is not supplied, making the system inoperable. The waveform I give in the attached Figure below + Schematic. I still have not found out where the system error is, I hope to receive help.
Regarding the waveform image, CH2 is VDD, CH3 is VDRV of the IC. It can be seen that when starting to supply VDRV pulse, VDD voltage drops and is not fed by VDD voltage from the auxiliary coil, because at this time the output voltage only fluctuates from 0 V -0.34 V. I have verified and confirmed that the converter operates normally when applying a fixed voltage of 15V to the VDD pin of the IC.
Fig. EXP. waveform
Schematic: Schematic