This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28750:ucc287502dbvr

Part Number: UCC28750


Tool/software:

Hello everyone. Using the UCC287502dbvr integration, I am making a flyback with 130v input 12v 6a output 72W output. But I get the output as 0. When I observe the supply of the input, I see that it is not fed. Obviously, I think that the start is not given for the integration to start. My primary winding is 42 secondary winding 8 aux 10 windings. Can you help with this issue?Schematic_Bitirme_Flyback_Converter_V1_2024-12-18.pdf