This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP9730: Load sharing among two Flyback power supplies using droop control

Part Number: PMP9730


Tool/software:

Hello all,

I am working on load sharing among two distinct flyback power supplies, each rated for nominal 12Vdc output and 3 Adc load (with current limiting at full load)

It is expected that the power supplies must share the common load in ORing configuration (typically 5A max) using output voltage droop control.

Can it me done with reference design PMP9730? Please suggest a method for implementation using the same or equivalent controller.

Any suggestions/ feedback is appreciated.

Regards,
Pratik N