TIDA-010938: Duration for output power to sustain during overloading

Part Number: TIDA-010938

Tool/software:

Hi SEM team, 

Regarding TIDA-010938, if the output power of the inverter is overloaded up to 125%, 150%, or more than 150%, how long (in seconds) will the output power sustain? Do we have this data?

For example:

  • 100% - 125%: How many seconds?
  • 125% - 150%: How many seconds?
  • More than 150%: How many seconds? 

Note: 100% refers to maximum continuous power (4.6kW)

Thanks.

Regards,

John