Part Number: TIDA-RESOLVER-APPLICATIONS-REFERENCE-DESIGN
Other Parts Discussed in Thread: TIDA-01527, TIDM-02014
Tool/software:
hi all
,
i am working on TIDA-01527 for insuring the smooth working of resolver. i have question relates to below circuit
because of input AM signal coming, differential amplifier does it pass directly or further circuits are filtering instead of passing only envelop because, R32 and C15 does only here as a bucket filter. i have to configure the resolver with sincos encoder. so, does the output of OSIN and OCOS is enough or any filter require in between of them. if yes, then how to calculate the parameter(cutoff frequency and filter order) for the smooth angle configuration?
best regard,
thankyou!