Part Number: LM5122
Other Parts Discussed in Thread: PMP21274
Tool/software:
Hello, I am trying to create a design for a boost converter using the LM5122 with the following requirements: Vin nom = 12, 10V<Vin<50; Iout nom =2.2A, 100mA<Iout<2.5A.
Power designer creates a design with Fsw=194kHz but shows constant duty cycle, unstable output voltage, strange inductor waveforms, requires 2x 180A low side Mosfets, requires a 36A inductor and throws an error when trying to export the design for Tina
I've varied the design parameters within reason but can't create a successful design, any idea what the trouble might be?
The design doesn't have to use the LM5122 but a high efficiency design >90% using a synchronous rectifier is preferred
Thanks, Ralph