Part Number: TIDA-01606
Other Parts Discussed in Thread: TIDA-010210, PMP22951
Tool/software:
Hello!
(Excuse me, I'm a a bit of a noob at power conversion, so sorry if this is a daft question).
I'm looking at building a 10kw, 3 phase bi-directional converter using 50V batteries for a bespoke application. High efficiency, high power density and short development time are important. Component cost is not.
I was reading SLAA602Awhich has an intriguing section about "high frequency" converters for better efficiency. See the attached figure

My questions are:
- Is there are reference design for such an topology? I haven't been able to find one. Is that because it's not really as good as expected?
- Is the more modern approach to have a bidirectional DC/DC stage coupled with a bidirectional DC/AC stage, with say 400V DC bus?
- If, so which of these reference designs is most suitable for the DC/AC stage: TIDA-01606 (T type) or TIDA-010210 - (ANPC) ? Or something else?
- For the DC/DC stage can I just put a few of these 3kw phase shifted full bridge ( PMP22951 ) in parallel? If not, what?
Cheers!