Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

LMG3522R030-Q1: Simulation or Loss analysis support on GaN with UCC28950-Q1 PSFB controller

Part Number: LMG3522R030-Q1
Other Parts Discussed in Thread: UCC28950-Q1,

Tool/software:

Hello Team,

I would like to use LMG3522R030-Q1 in OBC development using PSFB controller UCC28950-Q1.

SLUC222 design calculation sheet used to size magnetics & power train components.

Primary & Secondary side planning to use same device LMG3522R030-Q1. (Input 370V to 420V & output 80V to 120V, Pout 2500W). How to estimate SR FET loss?

Looking for Eon , Eoff & Ecoss loss parameter of LMG3522R030-Q1.

Thanks & Regards,

Babu S