This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP23338: code for the inverter mode or control logic that is used

Part Number: PMP23338
Other Parts Discussed in Thread: PMP23069

Tool/software:

Hi Team,

My Customer went through the the TI solutions for pmp23338,  and as per the document, the code for the inverter mode of pmp23338 was in the development process  If it is ready now, can you please share it ?

Or else if you could tell them the control logic used there (PI/PR controller for current and voltage loop etc.), it will help them in the development of VSI boards based on pmp23338 reference.

Thanks & Regards,

Manikya Sharma

  • Hi

    Apology for the delay in response.

    The code for inverter mode for pmp23338 is not developed yet. We have very similar reference design pmp23069. This one has inverter mode but only in grid-connected mode. You can check our old reference design TIEVM HV DC-AC. This one has VSI mode.

    Thank you

    Amir Hussain