Part Number: TIDA-050047
Other Parts Discussed in Thread: BQ25798, USB-PD-CHG-EVM-01, TPS25751, TPS25750
Tool/software:
Hi
Does TI have a PD Controller+Charger integrated IC?
Similar to Infineon: CYPM1115/1116
I can't find the integrated type on the TI official website, it seems that they are all 1 PD controller + 1 charger alone
https://www.ti.com/lit/ug/tiduey1b/tiduey1b.pdf?ts=1735785409207
The customer's design requirements are as follows
Does TI have a suitable solution?
battery capacity > 4.2v 10Ah, 3 strings
The key controller battery is charged > Type-c
Fast charging protocol> PD/QC30W ~45W Input: 5V/9V/12V/15V, 5A(max)
Charging time> about 1 hour (PD 30W ~45W fast charging)
Also TIDA-050047
The schematic on the reference design website can only be downloaded as a PDF file
Is there an Orcad DSN file?