This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01606: A Phase current sensing Noise Problem

Part Number: TIDA-01606
Other Parts Discussed in Thread: TMCS1123

Tool/software:

hello.

I am writing to ask a question about current sensing.

As shown in the current photo, I increased the input dc voltage to 500v.

I can see that the B-phase current and C-phase current are detected normally. However, it was confirmed that the A-phase current had severe ripples.(The photo on the left is the A-phase current, and the photo on the right is the B-phase current.)

It was confirmed that the current code uses the SDFM method, and as a result of measuring the SDFM output signals of phase A and phase B on the hardware, it was confirmed that there was no significant difference.(ex :SD_Data_IG_A)

Why is phase A sensing not working?

Thank you.